|
Welcome to the RAISE Software Installation page. As this is a new
way of installing the latest RAISE Software, there a some new
methods to get used to. The following describes the general
process of installing the RAISE Software for the first time using
this new method:
- Just by loading this page an InstallShield
" applet" may be
downloaded to run the installation script (unless it is already
installed on your system). This applet enables
internet-based installations.
- The InstallShield applet download may display a dialog box
asking if you want to accept the applet called "InstallShield
Wizard". Select "Yes" to accept it. Please wait for it
to be installed.
- Once this applet is installed, the
installation link will be changed from "Please
Wait..." to "Install".
When the link
changes to "Install", click on it.
- A pause of up to several minutes will occur while a connection
is made to download the installation package file.
- When an InstallShield Wizard "Authenticity
Verified" dialog box
appears, press the
"Next" button.
- The installation package file is then downloaded and evaluated
to determine what components are available to be installed.
Wait for the "Preparing Setup" dialog to complete.
- The Installation Welcome dialog will then appear. This
is the beginning of the RAISE Software installation.
- Follow the on screen instructions.
Note that you may be notified that you may need to update some
Internet Explorer components. Should this be true for your
system, you will be re-directed to
another web page to assist you with this additional installation.
Your download time will depend on the speed of your Internet connection and the number of files you select.
|